AXIS#.SWLS.EN

Description

Enables or disables software limit switches.

Software limit switches are active only if the axis has been homed.

Examples

Usage

0: Disable both software limit switches

1: Enable software limit switch 0, AXIS#.SWLS.LIMIT0

2: Enable software limit switch 1, AXIS#.SWLS.LIMIT1

3: Enable both software limit switches

 

If AXIS#.SWLS.EN = 3, then whichever limit switch is set to a greater value will be used as the upper limit switch. For all other values of AXIS#.SWLS.EN, use AXIS#.SWLS.LIMIT0 for the lower limit switch and AXIS#.SWLS.LIMIT1 for the upper limit switch.

Code

Axis 1 lower limit switch set to 1000 and upper limit switch set to 5000. Axis 1 home position is set and then both software limit switches are enabled.

-->AXIS1.SWLS.LIMIT0 1000

-->AXIS1.SWLS.LIMIT1 5000

-->AXIS1.HOME.SET

-->AXIS1.SWLS.EN 3

Context

For more information on limit switches, refer to Limits.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units N/A
Range 0 to 3
Default Value 0
Data Type Integer
See Also AXIS#.SWLS.STATE, AXIS#.SWLS.LIMIT0, AXIS#.SWLS.LIMIT1
Stored in Non Volatile Memory Yes

Variants Supported

All variants are supported

Fieldbus Information

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.SWLS.EN 0x500F 0x1 USINT - - RW False
AXIS2.SWLS.EN 0x510F 0x1 USINT - - RW False

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen